Keysight 89600 VSA .NET API
MultichannelAnalysisMode Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > CarrierMapping Class : MultichannelAnalysisMode Property


Glossary Item Box

Gets or sets a value indicating the multiple channel analysis mode for this carrier.

Syntax

Visual Basic (Declaration) 
Public Overridable Property MultichannelAnalysisMode As MultichannelAnalysisMode
C# 
public virtual MultichannelAnalysisMode MultichannelAnalysisMode {get; set;}
C++/CLI 
public:
virtual property MultichannelAnalysisMode MultichannelAnalysisMode {
   MultichannelAnalysisMode get();
   void set (    MultichannelAnalysisMode value);
}

Property Value

The default value is Mimo.

Remarks

When multiple channels are assigned to this carrier, if this value is MultichannelAnalysisMode.Mimo, the carrier is measured with multiple input channels; if this value is MultichannelAnalysisMode.Individual, the carrier is measured on each input channel independently. if this value is MultichannelAnalysisMode.MimoAndIndividual, besides the measurement with multiple input channels(normal MIMO measurement), it is also measured on each input channel independently. A new trace Demod Channel Summary is added to display the per channel measurement results for this carrier, so that user can view the following results on each individual channel: channel power, relative channel power, time offset, relative time error, evm, frequency error and symbol clock error.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.00

See Also