Keysight 89600 VSA .NET API
LteCrsRateMatchPattern Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : LteCrsRateMatchPattern Class

Glossary Item Box

The following tables list the members exposed by LteCrsRateMatchPattern.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyDownlinkCarrierBandwidthGets or sets a value indicating the LTE Carrier Bandwidth.  25.00
Public PropertyDownlinkCarrierFrequencyOffsetGets or sets a value indicating the LTE Carrier Center Frequency offset/>.  25.00
Public PropertyEnabledGets or sets a value indicating whether the RateMatchPattern around LTE CRS is enabled or not.  25.00
Public PropertyFourFramesSubframeAllocationGets or sets the LTE MBSFN subframe allocation in four frames.  25.00
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyMbsfnSubframeIndexesGets or sets the LTE MBSFN subframe indexes (zero-based).  25.00
Public PropertyNumberOfPortsGets or sets a value indicating the number of LTE CRS antenna ports.  25.00
Public PropertyOneFrameSubframeAllocationGets or sets the LTE MBSFN subframe allocation in one frame.  25.00
Public PropertyRadioFrameAllocationOffsetGets or sets the LTE MBSFN frame allocation offset.  25.00
Public PropertyRadioFrameAllocationPeriodGets or sets the LTE MBSFN frame allocation period.  25.00
Public PropertySubframeResourceTypeGets or sets the LTE MBSFN subframe resource allocation type.  25.00
Public PropertyVShiftGets or sets a value indicating the frequency mapping shift value for LTE CRS  25.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also