Keysight 89600 VSA .NET API
Enabled Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > LteCrsRateMatchPattern Class : Enabled Property


Glossary Item Box

Gets or sets a value indicating whether the RateMatchPattern around LTE CRS is enabled or not.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Enabled As Boolean
C# 
public abstract bool Enabled {get; set;}
C++/CLI 
public:
abstract property bool Enabled {
   bool get();
   void set (    bool value);
}

Remarks

When this value is true, all PDSCH resource mappings within this carrier need to rate match around the LTE CRS subcarriers/symbols. This value can be set as true when only numerology 15kHz is enabled for this carrier. If 15kHz numerology is not enabled or if other numerology is enabled, the value is false. Default value is false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also