| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property IsChannelFrequencyResponsePerSlot As Boolean | |
| C# | |
|---|---|
public virtual bool IsChannelFrequencyResponsePerSlot {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property bool IsChannelFrequencyResponsePerSlot { bool get(); void set ( bool value); } | |
Property Value
The default value is falseWhen this value is true, the channel frequency response is per slot channel frequency response, regardless of the EqualizerTrainingTimeBasis. When this value is false, the channel frequency response depends on EqualizerTrainingTimeBasis as below: if EqualizerTrainingTimeBasis is EqualizerTrainingTimeBasis.Slot, the channel frequency response is per slot channel frequency response, and the number of channel responses is the number of slot within the measurement interval; if EqualizerTrainingTimeBasis is EqualizerTrainingTimeBasis.Subframe, the channel frequency response is per subframe channel frequency response, and the number of channel responses is the number of subframe within the measurement interval; if EqualizerTrainingTimeBasis is EqualizerTrainingTimeBasis.Frame, the channel frequency response is per frame channel frequency response, and the number of channel responses is the number of frame within the measurement interval; if EqualizerTrainingTimeBasis is EqualizerTrainingTimeBasis.ResultLength, the channel frequency response is a single channel frequency response over the whole measurement interval;
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.40