Keysight 89600 VSA .NET API
SynchronizationCanUseMib Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : SynchronizationCanUseMib Property


Glossary Item Box

Gets or sets a value indicating whether synchronization may use MIB data

Syntax

Visual Basic (Declaration) 
Public Overridable Property SynchronizationCanUseMib As Boolean
C# 
public virtual bool SynchronizationCanUseMib {get; set;}
C++/CLI 
public:
virtual property bool SynchronizationCanUseMib {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true

Remarks

Setting this value to false may fix synchronization problems due to invalid MIB data present in SS/PBCH indexes of an analyzed signal. Setting this to true ensures certain synchronization scenarios have robust frame offset detection. This specifically helps cases where SSBlock.Lmax is Lmax.L8 or Lmax.L64 and SSBlock.Periodicity is Periodicity.Period5Milliseconds.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also