Gets or sets a value indicating whether measurement channel indexes mapping to each layer of this Pusch should be determined automatically.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property MeasurementChannelIndexesAuto As Boolean |
| C# | |
|---|
public virtual bool MeasurementChannelIndexesAuto {get; set;} |
| C++/CLI | |
|---|
public:
virtual property bool MeasurementChannelIndexesAuto {
bool get();
void set ( bool value);
} |
Property Value
The default value is true.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 29.00
See Also