| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub SetMeasurementChannelIndexes( _ ByVal ParamArray values() As Integer _ ) | |
| C++/CLI | |
|---|---|
public: virtual void SetMeasurementChannelIndexes( ... array<int>^ values ) | |
Parameters
- values
- The measurement channel indexes to associate with this carrier.
This CarrierMapping has a measurement center frequency of FrequencyOffset + Agilent.SA.Vsa.Measurement.Channels[(GetMeasurementChannelIndexes()[0])].Center. If a requested measurement channel cannot contain the carrier measurement frequency, the measurement channel index will not be used. If MeasurementChannelIndexesAuto is true, calling this method will force MeasurementChannelIndexesAuto to false. The measurement channel indexes associated with this CarrierMapping are available from GetMeasurementChannelIndexes.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00