Keysight 89600 VSA .NET API
IsValid Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > ResourceGrid Class : IsValid Property


Glossary Item Box

Gets a value indicating whether this resource grid is supported by 5G NR when the transmission bandwidth is specified. Please see MaximumTransmissionBandwidth.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property IsValid As Boolean
C# 
public abstract bool IsValid {get;}
C++/CLI 
public:
abstract property bool IsValid {
   bool get();
}

Property Value

The default value depends on MaximumTransmissionBandwidth and the index of this resource grid in the ResourceGridCollection. Index 0 represents Mu0:15kHz. Index 1 represents Mu1:30kHz. Index 2 represents Mu2:60kHz. Index 3 represents Mu3:120kHz. Index 4 represents Mu4:240kHz.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also