Gets or sets the size for this resource grid
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property Size As Integer |
| C# | |
|---|
public abstract int Size {get; set;} |
| C++/CLI | |
|---|
public:
abstract property int Size {
int get();
void set ( int value);
} |
Property Value
The default value depends on the index of this resource grid in the
ResourceGridCollection and the
MaximumTransmissionBandwidth. Index 0 represents Mu0:15kHz. Index 1 represents Mu1:30kHz. Index 2 represents Mu2:60kHz. Index 3 represents Mu3:120kHz. Index 4 represents Mu4:240kHz.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also