Keysight 89600 VSA .NET API
SubcarrierSpacingCommon Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > SSBlock Class : SubcarrierSpacingCommon Property


Glossary Item Box

Gets or sets the subcarrier spacing used for the SubcarrierOffset when ssb numerology is 120kHz or 240kHz.

Syntax

Visual Basic (Declaration) 
Public Overridable Property SubcarrierSpacingCommon As SubcarrierSpacingCommon
C# 
public virtual SubcarrierSpacingCommon SubcarrierSpacingCommon {get; set;}
C++/CLI 
public:
virtual property SubcarrierSpacingCommon SubcarrierSpacingCommon {
   SubcarrierSpacingCommon get();
   void set (    SubcarrierSpacingCommon value);
}

Remarks

according to the standard, when Numerology is 15kHz or 30kHz, RBOffset and SubcarrierOffset are always in 15Hz when Numerology is 120kHz or 240kHz, RBOffset is in 60kHz, SubcarrierOffset is in this common subcarrier spacing

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.20

See Also