Keysight 89600 VSA .NET API
GetSfiSymbolDirections Method
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > SearchSpace Class : GetSfiSymbolDirections Method


sfi
The slot format indicator to get the detailed symbol directions.

Glossary Item Box

Gets the slot format indicator symbol directions.

Syntax

Visual Basic (Declaration) 
Public Overridable Function GetSfiSymbolDirections( _
   ByVal sfi As Integer _
) As SfiSymbolDirection()
C# 
public virtual SfiSymbolDirection[] GetSfiSymbolDirections( 
   int sfi
)
C++/CLI 
public:
virtual array<SfiSymbolDirection>^ GetSfiSymbolDirections( 
   int sfi
) 

Parameters

sfi
The slot format indicator to get the detailed symbol directions.

Return Value

The array of symbol directions.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.20

See Also