| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property FrequencyHoppingBHop As Integer | |
| C# | |
|---|---|
public abstract int FrequencyHoppingBHop {get; set;} | |
Property Value
The value is defined in TS38.211 Table 6.4.1.4.3-1, it ranges from 0 to 3. The default value is 0.According to TS38.211 6.4.1.4.3, this value along with and decide whether frequency hopping is enabled and the frequency hopping pattern when frequency hopping is enabled.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00