Keysight 89600 VSA .NET API
FrequencyHoppingCSrs Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Srs Class : FrequencyHoppingCSrs Property


Glossary Item Box

Gets or sets a value indicating the bandwidth configuration of this physical channel.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FrequencyHoppingCSrs As Integer
C# 
public abstract int FrequencyHoppingCSrs {get; set;}
C++/CLI 
public:
abstract property int FrequencyHoppingCSrs {
   int get();
   void set (    int value);
}

Property Value

The value is defined in TS38.211 Table 6.4.1.4.3-1, it ranges from 0 to 63. The default value is 0.

Remarks

According to TS38.211 6.4.1.4.3, this value decide the total RB number available for SRS transmission. Also along with and , it decides the frequency hopping pattern of SRS.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also