Keysight 89600 VSA .NET API
FrequencyHoppingBSrs Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Srs Class : FrequencyHoppingBSrs Property


Glossary Item Box

Gets or sets a value indicating the frequency hopping b-SRS of this physical channel.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FrequencyHoppingBSrs As Integer
C# 
public abstract int FrequencyHoppingBSrs {get; set;}
C++/CLI 
public:
abstract property int FrequencyHoppingBSrs {
   int get();
   void set (    int value);
}

Property Value

The value is defined in TS38.211 Table 6.4.1.4.3-1, it ranges from 0 to 3. The default value is 0.

Remarks

According to TS38.211 6.4.1.4.3, this value along with and decide the frequency hopping pattern of SRS.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also