Keysight 89600 VSA .NET API
RepetitionFactor Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Srs Class : RepetitionFactor Property


Glossary Item Box

Gets or sets a value indicating the repetition factor of this physical channel.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property RepetitionFactor As SrsRepetitionFactor
C# 
public abstract SrsRepetitionFactor RepetitionFactor {get; set;}
C++/CLI 
public:
abstract property SrsRepetitionFactor RepetitionFactor {
   SrsRepetitionFactor get();
   void set (    SrsRepetitionFactor value);
}

Property Value

The repetition factor can 1 or 2 or 4. The default value is 1.

Remarks

According to TS38.211 6.4.1.4.3, this value along with other parameters decide the frequency position index when frequency hopping is enabled.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also