Gets or sets a value indicating whether per OFDM symbol phase compensation for the input data is enabled for the DirectCalculation.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Property SymbolPhaseCompensationEnabled As Boolean |
| C# | |
|---|
public bool SymbolPhaseCompensationEnabled {get; set;} |
| C++/CLI | |
|---|
public:
property bool SymbolPhaseCompensationEnabled {
bool get();
void set ( bool value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 28.40
See Also