Keysight 89600 VSA .NET API
CalculationControl Class Members
See Also  Properties 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace : CalculationControl Class

Glossary Item Box

The following tables list the members exposed by CalculationControl.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorCalculationControl ConstructorInitializes a new instance of the CalculationControl class.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAreDemodPropertiesOverriddenGets or sets a value indicating whether some of the demodulation properties are overridden.  —
Public PropertyBlockErrorRateEnabledGets or sets a value indicating whether BLER is calculated in the DirectCalculation.  —
Public PropertyDecodedBitsEnabledGets or sets a value indicating whether decoded bits are calculated in the DirectCalculation.  —
Public PropertyDecodeMaxIterationGets or sets a value indicating the maximum LDPC decode iteration in DirectCalculation.  —
Public PropertyEvmEnabledGets or sets a value indicating whether EVM is calculated in the DirectCalculation.  —
Public PropertyFrameTriggerEnabledGets or sets a value indicating whether the data is captured with frame trigger enabled for the DirectCalculation.  —
Public PropertyInputDataDomainGets or sets the input data domain for this DirectCalculation.  —
Public PropertyResultLengthInSubframeGets or sets a value indicating the result length in subframes for the DirectCalculation.  —
Public PropertySettlePointsAutoFilledWithZeroGets or sets a value indicating whether settling points are included in the input data.  —
Public PropertySymbolPhaseCompensationEnabledGets or sets a value indicating whether per OFDM symbol phase compensation for the input data is enabled for the DirectCalculation.  28.40
Public PropertyTimeDomainSignalCarrierCenterFrequencyGets or sets a value indicating the component carrier center frequency in Hz within the time domain input signal.  30.00
Public PropertyTimeDomainSignalCenterFrequencyGets or sets a value indicating the center frequency in Hz of the time domain input signal.  30.00
Public PropertyTimeDomainSignalSampleRateGets or sets a value indicating the sample rate in Hz of the time domain input signal.  28.40
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also