Keysight 89600 VSA .NET API
AllocationMode Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace > StandardSpecificConfiguration Class : AllocationMode Property


Glossary Item Box

Gets or sets how the carriers defined by the test model are configured in frequency.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AllocationMode As AllocationMode
C# 
public abstract AllocationMode AllocationMode {get; set;}
C++/CLI 
public:
abstract property AllocationMode AllocationMode {
   AllocationMode get();
   void set (    AllocationMode value);
}

Remarks

The default value is AllocationMode.Contiguous.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also