Keysight 89600 VSA .NET API
StandardSpecificConfiguration Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace : StandardSpecificConfiguration Class

Glossary Item Box

The following tables list the members exposed by StandardSpecificConfiguration.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAllocationModeGets or sets how the carriers defined by the test model are configured in frequency.  —
Public PropertyAssumedAdjacentChannelGets or sets the assumed adjacent channel.  —
Public PropertyBaseStationCategoryGets or sets the BS category.  —
Public PropertyBaseStationTypeGets or sets the BS mode.  —
Public PropertyCarrierConfigurationsGets the collection of carrier configurations use by this context.  —
Public PropertyCarrierIndexBeforeNoncontiguousBreakGets or sets the index of the last carrier before the non-contiguous allocation break.  —
Public PropertyCarrierReferenceFrequencyGets or sets the carrier reference frequency used when positioning CarrierConfigurations.  —
Public PropertyChannelRasterGets or sets the channel frequency raster for positioning the CarrierConfigurations.  —
Public PropertyChannelSpacingGets or sets the channel spacing of the CarrierConfigurations.  —
Public PropertyDuplexSchemeGets or sets the duplex scheme used by the test model.  —
Public PropertyFrequencyRangeLimitMaskGets or sets the frequency range limit mask.  —
Public PropertyFrequencyRangeLimitMaskAutoGets or sets a value indicating whether the FrequencyRangeLimitMask is automatically configured.  —
Public PropertyIntegrationBandwidthGets or sets the integration bandwidth of the component carriers in Hz.  —
Public PropertyIntegrationBandwidthAutoGets or sets a value indicating whether the integration bandwidth of the component carriers is automatically configured.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyLinkDirectionGets or sets the link direction used by the test model.  —
Public PropertyMaxTransmissionBandwidthGets or sets the transmission bandwidth used by the CarrierConfiguration.  —
Public PropertyNumerologyGets or sets the subcarrier spacing used by the CarrierConfiguration.  —
Public PropertySupportedModulationFormatForTM2And31Gets or sets the lower modulation format supported by this UE for test model 2 and test model 3.1 measurement.  25.40
Public PropertyTestModelNumberGets or sets the test model number configuration.  —
Public PropertyUEPowerClassGets or sets the UE power class.  —
Public PropertyUplinkChannelTypeGets or sets the uplink channel type.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodConfigureContiguousCarriersConfigures the number of CarrierConfigurations and their positions contiguously.  —
Public MethodConfigureNoncontiguousCarriersConfigures the number of CarrierConfigurations and their positions with 2 subblocks.  —
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also