| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property FrequencyRangeLimitMaskAuto As Boolean | |
| C# | |
|---|---|
public abstract bool FrequencyRangeLimitMaskAuto {get; set;} | |
The default value is true. Auto calculation is dependent on the CarrierReferenceFrequency, CarrierConfiguration.RelativeFrequency, and MaxTransmissionBandwidth. More specifically, the Carrier center frequency and Carrier Frequency Range are used to calculate the FrequencyRangeLimitMask.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)