| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IntegrationBandwidth As Double | |
| C# | |
|---|---|
public abstract double IntegrationBandwidth {get; set;} | |
The integration bandwidth defines the frequency range over which the integrated power is calculated. This value must not exceed the MaxTransmissionBandwidth of the component carrier. The default value is 100 MHz.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)