Keysight 89600 VSA .NET API
AntennaSpacing Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > AngleOfArrival Class : AntennaSpacing Property


Glossary Item Box

Gets or sets a value indicating the antenna spacing to use for each AoaAntenna.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AntennaSpacing As Double
C# 
public abstract double AntennaSpacing {get; set;}
C++/CLI 
public:
abstract property double AntennaSpacing {
   double get();
   void set (    double value);
}

Remarks

AntennaSpacing affects the AoaAntenna.XPosition and AoaAntenna.ZPosition of each antenna. Antenna spacing is in meters.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also