Gets or sets the input signal acquisition length for non-segmented capture.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property AcquisitionLength As Double |
| C# | |
|---|
public abstract double AcquisitionLength {get; set;} |
| C++/CLI | |
|---|
public:
abstract property double AcquisitionLength {
double get();
void set ( double value);
} |
Property Value
The units are seconds. The default value is 100 µs.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 19.00
See Also