| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property DeinterleaveByFrequency As DeinterleaveEmitterSelections | |
| C# | |
|---|---|
public virtual DeinterleaveEmitterSelections DeinterleaveByFrequency {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property DeinterleaveEmitterSelections DeinterleaveByFrequency { DeinterleaveEmitterSelections get(); void set ( DeinterleaveEmitterSelections value); } | |
Property Value
The default value is DeinterleaveEmitterSelections.None.This is a bitwise variable, so multiple emitters can be set if multiple bits are set on the value passed.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00