Gets or sets the pulse detection hysteresis relative to the detection
DetectionThreshold.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property DetectionHysteresis As Double |
| C# | |
|---|
public abstract double DetectionHysteresis {get; set;} |
| C++/CLI | |
|---|
public:
abstract property double DetectionHysteresis {
double get();
void set ( double value);
} |
Property Value
The default value is 1 dB.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 19.00
See Also