Keysight 89600 VSA .NET API
DetectionThreshold Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : DetectionThreshold Property


Glossary Item Box

Gets or sets the pulse detection threshold.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property DetectionThreshold As Double
C# 
public abstract double DetectionThreshold {get; set;}
C++/CLI 
public:
abstract property double DetectionThreshold {
   double get();
   void set (    double value);
}

Property Value

The default value is -10.

Remarks

The signal level must increase past this threshold to be detected as the rising edge of a pulse. See DetectionHysteresis for more information.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also