Keysight 89600 VSA .NET API
DetectionMaximumCount Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : DetectionMaximumCount Property


Glossary Item Box

Gets or sets the maximum number of pulses that will be detected when IsDetectionMaximumCountLimited is true.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property DetectionMaximumCount As Integer
C# 
public abstract int DetectionMaximumCount {get; set;}
C++/CLI 
public:
abstract property int DetectionMaximumCount {
   int get();
   void set (    int value);
}

Property Value

The default value is 100.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also