Keysight 89600 VSA .NET API
IsDetectionMaximumCountLimited Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : IsDetectionMaximumCountLimited Property


Glossary Item Box

Gets or sets a value indicating whether the number of pulses detected is limited by DetectionMaximumCount.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsDetectionMaximumCountLimited As Boolean
C# 
public abstract bool IsDetectionMaximumCountLimited {get; set;}
C++/CLI 
public:
abstract property bool IsDetectionMaximumCountLimited {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

This can be used to help ensure that consecutive measurements analyze the same number of pulses each time. This can also be useful to limit the maximum measurement analysis time when there is only noise present.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also