Keysight 89600 VSA .NET API
FrequencyReportMode Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : FrequencyReportMode Property


Glossary Item Box

Gets or sets whether frequencies in the result tables are absolute or relative to measurement center frequency.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FrequencyReportMode As FrequencyReportMode
C# 
public abstract FrequencyReportMode FrequencyReportMode {get; set;}
C++/CLI 
public:
abstract property FrequencyReportMode FrequencyReportMode {
   FrequencyReportMode get();
   void set (    FrequencyReportMode value);
}

Property Value

The default value is FrequencyReportMode.RelativeToCenter.

Remarks

When set to RelativeToCenter, frequencies in the result tables are relative to the measurement center frequency. When set to Absolute, frequencies in the result tables are absolute frequencies.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also