Keysight 89600 VSA .NET API
IsSelectedPulsesHighlighted Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : IsSelectedPulsesHighlighted Property


Glossary Item Box

Gets or sets a value indicating whether the selected pulses are highlighted on time-domain result traces.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsSelectedPulsesHighlighted As Boolean
C# 
public abstract bool IsSelectedPulsesHighlighted {get; set;}
C++/CLI 
public:
abstract property bool IsSelectedPulsesHighlighted {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

SelectedPulsesPart determines what parts of the pulse are highlighted.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also