Keysight 89600 VSA .NET API
SelectedPulsesPart Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : SelectedPulsesPart Property


Glossary Item Box

Gets or sets the parts of the pulse to show and highlight.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SelectedPulsesPart As SelectedPulsesPart
C# 
public abstract SelectedPulsesPart SelectedPulsesPart {get; set;}
C++/CLI 
public:
abstract property SelectedPulsesPart SelectedPulsesPart {
   SelectedPulsesPart get();
   void set (    SelectedPulsesPart value);
}

Property Value

The default value is Automatic.

Remarks

Note that the default value in version 19.00 was EntirePulse, while the default value in version 20.00 and beyond is Automatic. Automatic means amplitude-related traces and Acquisition Time use EntirePulse, while FM and phase-related traces use FrequencyPhaseAnalysis.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also