Keysight 89600 VSA .NET API
MeasurementPauseMetric Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : MeasurementPauseMetric Property


Glossary Item Box

Gets or sets what metric is used in pause on measurement.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property MeasurementPauseMetric As TableMetric
C# 
public abstract TableMetric MeasurementPauseMetric {get; set;}
C++/CLI 
public:
abstract property TableMetric MeasurementPauseMetric {
   TableMetric get();
   void set (    TableMetric value);
}

Property Value

The default value is TopLevel.

Remarks

You can set the measurement up to pause based on the relationship of measured value (or its absolute value) to a threshold value. The relation can be any of greater than, greater than or equal, less than, less than or equal, equal, or not equal.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also