Gets or sets the keep-out time for time sidelobe calculations, when
SidelobeKeepOutMode is
SidelobeKeepOutMode.Time.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property SidelobeKeepOutTime As Double |
| C# | |
|---|
public virtual double SidelobeKeepOutTime {get; set;} |
| C++/CLI | |
|---|
public:
virtual property double SidelobeKeepOutTime {
double get();
void set ( double value);
} |
Property Value
The units are seconds. The default value is 0.0 seconds.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 23.20
See Also