Keysight 89600 VSA .NET API
TopBaseCalculationMethod Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : TopBaseCalculationMethod Property


Glossary Item Box

Gets or sets the calculation method used for determining the top and base levels of pulses.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property TopBaseCalculationMethod As TopBaseCalculationMethod
C# 
public abstract TopBaseCalculationMethod TopBaseCalculationMethod {get; set;}
C++/CLI 
public:
abstract property TopBaseCalculationMethod TopBaseCalculationMethod {
   TopBaseCalculationMethod get();
   void set (    TopBaseCalculationMethod value);
}

Property Value

The default value is Median.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also