Keysight 89600 VSA .NET API
FrequencyMeanBaseError Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > TrainBaseError Class : FrequencyMeanBaseError Property


Glossary Item Box

Gets or sets the base error value, used for scoring, for the Frequency Mean metric.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FrequencyMeanBaseError As Double
C# 
public abstract double FrequencyMeanBaseError {get; set;}
C++/CLI 
public:
abstract property double FrequencyMeanBaseError {
   double get();
   void set (    double value);
}

Remarks

Train Scoring of Frequency Mean is calculated based on this error value.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also