Keysight 89600 VSA .NET API
TrainBaseError Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace : TrainBaseError Class

Glossary Item Box

The following tables list the members exposed by TrainBaseError.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyFMSlopeBaseErrorGets or sets the base error value, used for scoring, for the FM Slope metric.  —
Public PropertyFrequencyMeanBaseErrorGets or sets the base error value, used for scoring, for the Frequency Mean metric.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsFMSlopeEnabledGets or sets a value indicating whether the FM Slope metric for train scoring calculation is enabled.  —
Public PropertyIsFrequencyMeanEnabledGets or sets a value indicating whether the Frequency Mean metric for train scoring calculation is enabled.  —
Public PropertyIsModulationTypeEnabledGets or sets a value indicating whether the Modulation Type metric for train scoring calculation is enabled.  —
Public PropertyIsPriEnabledGets or sets a value indicating whether the PRI metric for train scoring calculation is enabled.  —
Public PropertyIsTopLevelEnabledGets or sets a value indicating whether the Top Level metric for train scoring calculation is enabled.  —
Public PropertyIsWidthEnabledGets or sets a value indicating whether the Width metric for train scoring calculation is enabled.  —
Public PropertyPriBaseErrorGets or sets the base error value, used for scoring, for the PRI metric.  —
Public PropertyTopLevelBaseErrorGets or sets the base error value, used for scoring, for the Top Level metric.  —
Public PropertyWidthBaseErrorGets or sets the base error value, used for scoring, for the Width metric.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also