Keysight 89600 VSA .NET API
Standard Property
See Also 
Agilent.SA.Vsa.Rfid.Interfaces Assembly > Agilent.SA.Vsa.Rfid Namespace > MeasurementExtension Class : Standard Property


Glossary Item Box

Gets the standard with which the current setting is comply

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property Standard As Standard
C# 
public abstract Standard Standard {get;}
C++/CLI 
public:
abstract property Standard Standard {
   Standard get();
}

Remarks

This value is equal to the newStandard in the most recent call of Preset(Standard newStandard).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also