Keysight 89600 VSA .NET API
RelativeFrequency Property
See Also 
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace > Carrier Class : RelativeFrequency Property


Glossary Item Box

Gets or sets the carrier center frequency (in Hz) as an offset from the MeasurementExtension.CarrierReferenceFrequency.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property RelativeFrequency As Double
C# 
public abstract double RelativeFrequency {get; set;}
C++/CLI 
public:
abstract property double RelativeFrequency {
   double get();
   void set (    double value);
}

Property Value

The default value is 0 Hz.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also