Gets or sets the reference frequency. Units are in Hz.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property CarrierReferenceFrequency As Double |
| C# | |
|---|
public abstract double CarrierReferenceFrequency {get; set;} |
| C++/CLI | |
|---|
public:
abstract property double CarrierReferenceFrequency {
double get();
void set ( double value);
} |
Property Value
Default value is 1 GHz.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also