Keysight 89600 VSA .NET API
DvbModulationCoding Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > Allocation Class : DvbModulationCoding Property


Glossary Item Box

Gets or sets the DVB-S2/S2X modulation/coding, which defines the constellation and bit mapping.

Syntax

Visual Basic (Declaration) 
Public Overridable Property DvbModulationCoding As DvbModulationCoding
C# 
public virtual DvbModulationCoding DvbModulationCoding {get; set;}
C++/CLI 
public:
virtual property DvbModulationCoding DvbModulationCoding {
   DvbModulationCoding get();
   void set (    DvbModulationCoding value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00

See Also