Keysight 89600 VSA .NET API
EndsAtEndOfFrame Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > Allocation Class : EndsAtEndOfFrame Property


Glossary Item Box

Gets or sets a value indicating whether this allocation ends at the end of the frame.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property EndsAtEndOfFrame As Boolean
C# 
public abstract bool EndsAtEndOfFrame {get; set;}
C++/CLI 
public:
abstract property bool EndsAtEndOfFrame {
   bool get();
   void set (    bool value);
}

Remarks

EndSymbolIndex and Length are determined automatically when EndsAtEndOfFrame = true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also