Keysight 89600 VSA .NET API
SynchronizationEnabled Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > Allocation Class : SynchronizationEnabled Property


Glossary Item Box

Gets or sets a value indicating whether Allocation is used for synchronization.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SynchronizationEnabled As Boolean
C# 
public abstract bool SynchronizationEnabled {get; set;}
C++/CLI 
public:
abstract property bool SynchronizationEnabled {
   bool get();
   void set (    bool value);
}

Remarks

Only used when SynchronizationMode = SynchronizationMode.Customized. Not applicable for AllocationType.Idle segments.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also