Keysight 89600 VSA .NET API
EqualizerReset Method
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > CarrierAggregation Class : EqualizerReset Method


Glossary Item Box

Reset the adaptive equalization coefficients as a single point impulse response for the carriers

Syntax

Visual Basic (Declaration) 
Public Overridable Sub EqualizerReset() 
C# 
public virtual void EqualizerReset()
C++/CLI 
public:
virtual void EqualizerReset(); 

Remarks

This is a one shot operation, when AdaptiveEqualizerMode is AdaptiveEqualizerMode.Track, after this function is called, the tracking will restart from the single point impulse response.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also