Keysight 89600 VSA .NET API
ReferenceFrequencyDefinition Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > CarrierAggregation Class : ReferenceFrequencyDefinition Property


Glossary Item Box

Gets or sets a value indicating the reference frequency definition for each component carrier.

Syntax

Visual Basic (Declaration) 
Public Overridable Property ReferenceFrequencyDefinition As ReferenceFrequencyDefinition
C# 
public virtual ReferenceFrequencyDefinition ReferenceFrequencyDefinition {get; set;}
C++/CLI 
public:
virtual property ReferenceFrequencyDefinition ReferenceFrequencyDefinition {
   ReferenceFrequencyDefinition get();
   void set (    ReferenceFrequencyDefinition value);
}

Remarks

If ReferenceFrequencyDefinition.AssignedMeasurementChannelCenter, the reference frequency of each component carrier is defined to be the center of the first measurement channel assigned to that component carrier. If no measurement channel is assigned to a component carrier, the ReferenceFrequency will be used as the reference frequency for that component carrier. If ReferenceFrequencyDefinition.ManuallySpecified, the reference frequency for all the component carriers is manually specified with ReferenceFrequency. ReferenceFrequency, ReferenceFrequencyDefinition, CenterFrequency, OffsetFromReferenceFrequency

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.40

See Also