Gets or sets a value indicating whether the frame has variable length (
Style =
FrameDefinitionStyle.Burst) for the carriers. See
FrameDefinition.VariableLengthEnabled for the carriers. The getter gets the value from the first carrier and the setter sets the value for all carriers.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property VariableLengthEnabled As Boolean |
| C# | |
|---|
public virtual bool VariableLengthEnabled {get; set;} |
| C++/CLI | |
|---|
public:
virtual property bool VariableLengthEnabled {
bool get();
void set ( bool value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 26.00
See Also