Keysight 89600 VSA .NET API
FrequencyEstimationMode Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > ComponentCarrier Class : FrequencyEstimationMode Property


Glossary Item Box

Gets or sets the FrequencyEstimationMode, which determines whether the frequency error is estimated and compensated.

Syntax

Visual Basic (Declaration) 
Public Overridable Property FrequencyEstimationMode As FrequencyEstimationMode
C# 
public virtual FrequencyEstimationMode FrequencyEstimationMode {get; set;}
C++/CLI 
public:
virtual property FrequencyEstimationMode FrequencyEstimationMode {
   FrequencyEstimationMode get();
   void set (    FrequencyEstimationMode value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also