Keysight 89600 VSA .NET API
ResetEqualizer Method
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > SingleCarrier Class : ResetEqualizer Method


Glossary Item Box

Reset the adaptive equalization coefficients as a single point impulse response

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub ResetEqualizer() 
C# 
public abstract void ResetEqualizer()
C++/CLI 
public:
abstract void ResetEqualizer(); 

Remarks

This is a one shot operation, when AdaptiveEqualizerMode is AdaptiveEqualizerMode.Track, after this function is called, the tracking will restart from the single point impulse response.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also