Keysight 89600 VSA .NET API
PredistortionMode Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > WaveformGeneration Class : PredistortionMode Property


Glossary Item Box

Gets or sets the waveform predistortion mode.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PredistortionMode As WaveformPredistortionMode
C# 
public abstract WaveformPredistortionMode PredistortionMode {get; set;}
C++/CLI 
public:
abstract property WaveformPredistortionMode PredistortionMode {
   WaveformPredistortionMode get();
   void set (    WaveformPredistortionMode value);
}

Remarks

When WaveformPredistortionMode.Off, no predistortion is applied to the waveform; when WaveformPredistortionMode.MeasuredChannelResponse, the waveform is predistorted with the measured channel response;

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.00

See Also