The following tables list the members exposed by WaveformGeneration.
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | AwgnAdded | Gets or sets a value indicating whether awgn is added to the waveform. | 30.00 |
![]() | CarrierToNoiseRatio | Gets or sets the carrier to noise ratio in dB when awgn is added to the waveform. | 30.00 |
![]() | IsDisposed | Gets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | OversampleRatio | Gets or sets the oversample ratio of the waveform. | 30.00 |
![]() | PostsignalIdleLength | Gets or sets the idle length in number of symbols after the signal part in the waveform. | 30.00 |
![]() | PostsignalIdleLengthAuto | Gets or sets a value indicating whether the idle length after the signal part is automatically determined or not. | 30.00 |
![]() | PredistortionMode | Gets or sets the waveform predistortion mode. | 30.00 |
![]() | PresignalIdleLength | Gets or sets the idle length in number of symbols before the signal part in the waveform. | 30.00 |
![]() | PresignalIdleLengthAuto | Gets or sets a value indicating whether the idle length before the signal part is automatically determined or not. | 30.00 |
![]() | SignalLength | Gets or sets the length in number of symbols of the active data part in the waveform. | 30.00 |
![]() | SignalLengthAuto | Gets or sets a value indicating whether the waveform length is automatically determined or not. | 30.00 |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | CreateObjRef | Creates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject) | — |
![]() | ForceRebuildKeyMap | This method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | GetLifetimeService | Retrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject) | — |
![]() | InitializeLifetimeService | Obtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | PropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | PropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemotePropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemotePropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | 14.00 |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||