Measurement Offset (802.16 OFDM)
: Zero (See 802.16 OFDM Standard Setups/Presets Table.)
is set in symbol-times. determines the start position of the with respect to first Symbol-time within the Result Length. See Measurement Interval and Offset for more information about this parameter and its application. The value must be less than the Result Length or Maximum Result Length parameter (depending on the which option is selected for Result Length). This parameter combined with Measurement Interval specifies the portion of the result length to analyze and display to the user.
See Also
Maximum Result Length (802.16 OFDM)
Result Length Parameters (802.16 OFDM)